Application Reports of Vacuum Clamping Systems
The examples of applications in various areas and sectors of trade and industry give you an impression of the possible uses of our vacuum clamping systems.
Clamping Device for the Aerospace Industry
The picture shows the usage of the vacuum clamping system matrix-plate at the metal processing in the aerospace industry. The often very complex geometry of parts used in the aerospace industry frequently require the use of clamping solutions matched specifically to the application. Maximum precision and careful handling of the workpieces are also very important.
The clamping of narrow and curved workpieces with Innospann adapter console
The Innospann adapter console is suitable for mounting on all Schmalz console systems. This system considerably improves the clamping of narrow and curved workpieces.
Vacuum Clamping System for the Flexible Handling of Different Workpieces
Vacuum Clamping System Multi-Clamp VC-M can be used on almost eyery surface so it´s flexible applicable in facilities and construction sites.
Woodworking Centre with Innospann Steel Plate
The application shows the vacuum clamping system Innospann Steel-Plate T integrated at a CNC woodworking centre. The Steel-Plate-T permits workpieces to be changed on one side while another workpieces is being machined on the other side, or even conversion of one side for a different workpiece, without interrupting operations.
Efficient Clamping of Aluminium Cubes
This application shows a Matrix-Plate in use on a CNC machining centre. It is secured to the machine table with the aid of mechanical clamping elements. The use of vacuum makes it possible to clamp the thin bases of the workpieces precisely and without distortion for five-axis machining without repositioning.
Individual Clamping of Wooden and Plastics Parts
The picture shows a CNC working centre with integrated Vacuum Clamping Systems VC-K2 which is used in the wood and plastic processing. A combination of the vacuum clamping systems VC-K2 and Innospann cares for the processing of the wide range of workpieces in one-off and small-batch parts.
Search
Extended searchAvailability and price check
Vacuum components, clamping systems and workshop equipment
Direct order
Shopping cart
Schmalz Media Center
You can find application videos for various industries demonstrating our vacuum tube lifters and vacuum lifting devices in the Schmalz Media Center.
More...