Application Reports of Vacuum Components
The examples of applications in various areas and sectors of trade and industry give you an impression of the possible uses of our vacuum components.
Foil-/Paper suction pads SGPN for handle non-rigid packed products
The flat suction pads SGPN are especially created for handling with various packing materials(plastic foils, paper, blister-packed). Through his flat, long-tapered sealing lip he has good sealing properties.
Compact Ejectors with an Integrated Field-Bus Interface in Press Shop
The Compact Ejector Schmalz-X-Pump with DeviceNet interface for the direct integration in fild-bus system reduces the installation effort. The use of a conventional I/O interface between fild-bus system and vacuum generator and the associated wiring is no longer necessary.
Precise Handling of Windows in the Automobile Industry
The suction pads of the type PFYN 95 VU1 generate very high and reliable holding force for precise positioning. They are made of hard-wearing a crack-resistant Vulkollan.
Vacuum Suction Pads SAB within the Automotive Press Plant
Vacuum components allow secure and exact handling of car body parts made of metall sheets. Within automotive press plants, highest demands on dynamics and cycle times are required.
Fight Against the „Cost-Eaters“ in Press Shops
High performance Schmalz X-Pump ejectors are eliminating tooling errors and are reducing costs in the handling of sheet-metal in the press shop of a big world wide car manufacturer
Removal of hot plastic parts from injection-moulding machines
Removal of hot plastic parts from injection-moulding machines with Suction Pad FSG-HT1
Flat Suction pads PFY for handling CDs/DVDs
The Flat suction pad PFY7 is specially made for sensitive workpieces with a smooth surface. Particularly it is suitable for workpieces which are made of silicon and polyurethan. It is often used for the safe and easy handling of CDs and DVDs. Using four vacuum pads increases the suction power.
Versatile modular system for linking of presses
The vacuum spider has adjustable arms, combined with the special sheet-metal suction pads SAB mounted on adjustable-height spring plungers, permits a highly flexible adaptation to a wide range of tasks.
Sensitive handling of blister packs
The demands placed on Vacuum Suction pads for the handling of blister packs are growing constantly. With ever thinner films, the trend is toward ever shorter cycle times. Here pads are required to avoid damage to the films even at high vacuum levels. In the present case, the realization using Suction pads SGPN made of natural rubber.
Modular Schmalz Vacuum Components for Complete Handling Solutions
The picture shows a vacuum gripper consisting of one longitudinal beam and eight cross-beams, all made of aluminium section which also act as a vacuum reservoir.
CD Handling with Bellows Suction Pad FGA PVC (1,5 folds)
For handling of CD / DVD with suction hub, the bellows suction pad FGA with 1,5 folds made of PVC is the optimal suction pad. Through its folds it ensures an optimal damping effect when touching down on the CD, and so ensures gentle handling. The large effectiv diameter provides high suction power and thus enables high acceleration and short cycle times. Since discs can be handled only on the blank inside edge, the outer diameter of the suction pad is voted on the inside edge of the blank CD.
Rational Rotating of Caravan Elements with Vacuum Components
The application shows the safe and rational turning of prefabricated side walls and roof modules for mobile homes and caravans.
Precise handling in press feeders
The photograph shows a complete press feeder SPEED SHUTTLE of Fibro with the vacuum spider mounted on it. An important requirement on the feeder and also on the vacuum gripper is that the metal sheets must remain in the specified position during transport.
Safe and fast handling of cardboard boxes and semi-flexible packaging
The bellows suction pads SPB1 are perfect for handling cardboard boxes and semi-flexible packaging. These suction cups are especially used in box and tray erectors, top and sideloading machines and palletizing processes.
Handling of abrasive and flexible card boardboxes
The handling of extremely abrasive (e.g. rough cardboard sheets) and unstable workpieces (e.g. rough cardboard) belongs to the daily tasks of the packaging industry. This processes can be automated by the high suction force of the oval Bellows suction pads SPOB1.
Gentle Handling of wafers and cells with the wafer gripper SWG
The wafer gripper SWG was specifically developed for the solar industry. It handles wafers and cells in the whole production process. In particular, it is used for the rapid loading and unloading. There, it removes the workpieces from boxes or conveyors, transports it through a camera and then puts the workpieces down in another box or conveyor.
Handling of film-packed products with Rectangular suction pads
Handling of film-packed products with Bellows suction pads FSGB-R (rectangular)
Search
Extended searchAvailability and price check
Vacuum components, clamping systems and workshop equipment
Direct order
Shopping cart
Schmalz Media Center
You can find application videos for various industries demonstrating our vacuum tube lifters and vacuum lifting devices in the Schmalz Media Center.
More...