Application stories of vacuum gripping systems - Schmalz

Application Reports of Vacuum Gripping Systems

The examples of applications in various areas and sectors of trade and industry give you an impression of the possible uses of our vacuum gripping systems.


Search results 38 aus 76

Vacuum Suction Spider SSP-SG

Safe Handling of Solar Glass and Solar Modules

The application describes the safe handling of solar glass and solar modules. The partly at the back side curved solar glass modules are fixed by using the vacuum technology for further processing stages such as framing and film cutting.

Palettizing and depalettizing with SPZ

Vacuum Layer Gripper SPZ

The vacuum layer gripper SPZ is the gripper system in palett size. This enabled the palettizing and depalettizing of whole product layers. This reduces significantly the cycle time.The suction plane is made of specially foam or single suction pads. Thereby the gripper adapts perfectly to the workpiece and it needs no gripper chance for various workpieces.

VacuGrip FX

More Flexibility Thanks to an Intelligent Gripping System

Rational handling of cardboard boxes and empty pallets thanks to a universal, modular, large-area vacuum gripper system

Large-area vacuum gripping system FX-SW

Palletising and Depalletising of Chipboards

Palletising and depalletising of chipboards. Improved flexibility with the large-area vacuum gripping system FX-SW in the automated handling of furniture elements. A large-area vacuum gripping system FX-SW, mounted on an industrial robot, being used to handle coated sheets of chipboard. Mounted on a Kuka industrial robot, the large-area vacuum gripping system FX-SW, used here to load an edge-gluing machine with material, offers a high level of flexibility and performance.

FXC for use with tabletop saw

Large-area gripping system FXC for use with tabletop saw

Sawing of wood panels is a dangerous and accurate work. The Warsaw Machinery company integrates into their automated saw systems, the large-area gripping system FXC. It enabled the handling for various workpieces in undefined positions.

Packaging Material Handling with SPZ-M-C

Handling of packages with the Vacuum Layer Gripper SPZ-M-C

The vacuum layer gripper SPZ-M-C was designed to handle a variety of packaging materials. The patented curtain concept and the manual clamping generate additional forces.

Handling of aluminum section with FMC

Handling of aluminium profiles with the Large-Area Vacuum Gripping System FMC

The large-Area Vacuum Gripping System FMC is optimum for handle aluminum sections. The number of aluminum sections per layer varies. That is not a problem for the FMC, because it the gripper system operates with full or partial occupancy.

VacuBox with two valve beams used for moving layers of timber

Moving Complete Layers of Timber

The classical VacuBox permits the safe and reliable handling of rough-sawn timber, warped or twisted beams, planks and boards with rough-sawn surfaces and even new and used pallets.

Press feeder for use in the bodywork press shop of an automobile manufacturer.

Vacuum gripper solution for press feeders

A good example of the system solutions offered by Schmalz is a press feeder for use in the bodywork press shop of an automobile manufacturer. This feeder was designed and built specifically for a project, in cooperation with Messrs. Zollern-Automation in Herbertingen, the supplier of the complete press-automation system.

Large-area vacuum gripping system SBX for handling timber

Large-area vacuum gripping system SBX for handling timber

The handling of timber in layers with rough surface can be done with the area vacuum gripping system. The area vacuum gripping system can also work with partial occupancy so that knoteholes not affect the handling and not complete layers can be smooth transported.

Door handling with large-area vacuum gripping system FXC

Door handling with large-area vacuum gripping system FXC

The large-area vacuum gripping system FXC is often used for the handling of doors. The FXC enabled the gripping of doors without damage and marking. The gripping system put down the doors on exactly position.Moreover, it can put spacer between the doors.

Double FX large-area vacuum gripping system

Safe Handling of Facing Panels

On the facing panels to be lifted, the available gripping surface is restricted by the geometry of the workpieces and the many openings. At the same time, the position of the area which can be gripped is not precisely defined.

Production-automation with the VacuBox

VacuBox System Solution

The VacuBox is a complete vacuum gripper system which is optimised to meet the complex demands of the woodworking industry, namely the fully automatic handling of layers of boards, laths and beams. It is designed for continuous operation and provides a rational solution to the existing problems.

Palletizing with the double vacuum beam SBX

Palletizing Extra-Strong Vacuum Beam SBX

The application video shows two different operations implemented with the aid of a vacuum beam of the type SBX1200x200. The first part of the video shows a palletizing operation with the aid of an industrial robot which grips a layer of several long wooden laths, moves them and stacks them on a pallet. The system is capable of handling workpieces of varying lengths and widths, even if they have cracks or knot-holes in their surfaces.

Moving layers of wood with the large-area gripping system FX .

Flexible Handling of Layers of Wood

The application video shows how several layers of individual wooden boards can be handled quickly and variably with a large-area gripping system of the type FX400x120, although there are sometimes cracks, knot-holes, etc. on the gripping surface.

Gripping System VacuBox

Gripping System VacuBox - Ideal for Moving Timber

Gripping System from Schmalz is a flexible, modular vacuum-gripper system for the handling of sawn timber.

Large-area vacuum gripping system FX 120/60

Handling of Structured Furniture Parts

This application example shows the fully automatic handling of structured furniture parts with varying dimensions with the aid of the large-area vacuum gripping system FX 120/60, which permits the activation and deactivation of specific suction zones. The flexible, hard-wearing sealing mat ensures damage-free handling of the parts. The presence of parts is monitored with an electronic vacuum sensor, permitting optimisation of the cycle times.

Pallet handling in refrigerated areas with vacuum layer gripper SPZ-M-Cool

Layerwise Handling in Refrigerated Areas with Layer Gripping System SPZ-M-Cool

The vacuum layer gripper SPZ-M-Cool has been designed for use in refrigerated areas.

Safe and economical handling of sawn timber

VacuBox Vacuum-Handling System for Layers of Sawn Timber

With its patented technology and flexible construction, the new VacuBox from Schmalz offers decisive benefits for the movement of layers of wood. A VacuBox vacuum-handling system makes it possible to handle layers of sawn timber consisting of very wide and heavy or very narrow (at least 40 mm) and light boards safely and economically.

Vacuum Gripping System for Robot- Assisted Handling of Furniture Parts

Vacuum Gripping System for Robot- Assisted Handling of Furniture Parts

This application example shows the complete vacuum gripper system, with spring-mounted suction pads, for the robot-assisted handling of furniture parts. The gripper system is used for the fully automatic loading of a machine which applies edge bands to the parts. The necessary vacuum is generated by a multi-chamber ejector of the type SEM.

Large-area vacuum gripping system SPZ-M for handling liquid package

Layer Gripping System SPZ-M handels Liquid Packages

Large-area vacuum gripping system with mechanical clamping for handling liquid package

Handling a Euro pallet

Fully Automatic Handling of Pallets and Cardboard Boxes

This example shows the transport of empty Euro pallets to a position where they are automatically loaded with cardboard boxes. The pallets are lifted with the aid of a large-area gripping system of the type FX600x80SW, mounted on a four-axis industrial robot manufactured by Messrs Fresenius Medical Care. The pallet is gripped along the centre board.

Veneer handling with vacuum spider SSP

Veneer handling with vacuum spider SSP

The seperate handling of veneer makes high demands on the careful handling. The vacuum spider SSP is best suited for this task.

Handling magazines and newspapers with SPZ-M-C

Large-area vacuum gripping system SPZ-M-C for handling magazines and newspapers

The automated handling of newspapers and magazines in layers is a difficult process. Because of the different layers, the uneven surface and the astable material, the newspaper were previously manuell or with more expenses transported.

The VacuBox unstacking layers of wood

The VacuBox from Schmalz - a Clever Solution

The removal of layers of boards, laths and planks from a stack is now child's play. The system is capable of handling workpieces of varying dimensions and weight made of different types of wood and arranged in different ways on the stack. Rough-sawn, unedged, cracked and warped workpieces can also be transported quickly and safely.

Handling of doors with the vacuum-area gripper system SBX

Area gripper system SBX enables automated handling of doors

The doors factory uses many machines. These machines must be quickly and accurately loaded. The Loading can be automated with the area gripper system SBX. The SBX enables automated palletizing and depalletizing the doors. The doors are carefully handled.

Vacuum Gripping System

Handling of Plastic Parts

The bellows-type suction pads FSG with 2.5 corrugations, made of hard-wearing NBR or heat-resistant silicone, are mounted on a handling unit of the type Multilift H made by Messrs. Arburg for the handling of injection-moulded parts. Depending on the task, the vacuum is supplied by one or two compact ejectors of the series SCPM MiniPump on each complete gripper system.

Vacuum spider SSP for handling checker plate

Vacuum spider SSP for handling checker plate

The vacuum spider SSP with the FMC-grippers is often used for handling cheker plate. The grippers have a low height and have a low weight. This makes them ideal for automated handling. Moreover, they have excellent sealing properties and absorb the unevenness of the checker plate.

Vacuum Spider for Carton Handling

Schmalz Vacuum Gripping System for Handling Cardboard Separators

The vacuum spiders consist of cross-beams made of aluminium sections, compact ejectors to provide the vacuum, spring plungers to compensate for any unevenness and bellows-type suction pads for gentle application to the workpieces. The system is thus ideal for careful and problem-free handling of cardboard separators, from picking up from the stack to placing in the correct position.

Handling of pallets with SBX

Pallet handling with vacuum gripping system SBX

The vacuum gripping system SBX enabled the automated handling of pallets. It lifts the empty pallet from the conveyor and put it down on the stack. This process ist fast and safety. Low pollution of the pallets affects not the process. The gripping, conversion and position of the pallets is compared with the same vacuum gripper.

Handling of boxes with FXC-SG

Large-area vacuum gripping system FXC-SG for handling cardboard

The large-area vacuum gripping system FXC-SG enables the flexible handling of cardboard boxes. The system operates with full or partial occupancy, so it can be handled a different number of cardboard.

Large-area vacuum gripping system FX

Vacu Gripping System FX in Practical Use

The photograph shows a vacuum gripper FX-35 which is used by Messrs. Trapo AG Fördertechnik for loading conveyor belts. Even if not fully in contact with the load, the FX-35 is capable of handling the goods safely, precisely and quickly. It is. for example, also capable of picking up single tin cans. Since the system can handle partial loads and is also suitable for use with many different objects, such as tin cans, cardboard boxes and pallets, it is extremely flexible.

Palettizing with SPZ-M

Palletizing and depalettizing with vacuum layer gripper SPZ-M

Palletizing and depalettizing from whole product layers with vacuum layer gripper SPZ-M with mechanical gripper assistance. The vacuum layer gripper SPZ ist the gripper system in palett size. This enabled the palettizing and depalettizing of whole product layors. This reduces significantly the cycle time.

Quadruple large-area gripping system FX

Fully Automatic Handling of Wooden Pallets of Different Sizes

Wooden pallets of varying sizes can be transported with the aid of the large-area gripper of the type FX mounted on an industrial robot. The position of the area on the pallet which can be gripped is undefined. In some cases, the available gripping area is reduced by the presence of cracks, knotholes, etc. The check valves of the large-area gripper FX ensure the maximum possible holding force on the available area, since they prevent leaks through vacuum inlets which are not in contact with the pallet.

VacuBox for moving complete layers of wooden planks

Moving Complete Layers of Wooden Planks

When moving layers of wooden planks, the overall width of a layer may not exceed 1000 mm. Depending on the order to be filled, only a defined number of planks is lifted, and this is often less than the total number of planks in one layer. In extreme cases, it must be possible to grip only a single plank securely.

Quadruple large-area vacuum gripping system FX

Fully Automatic Stacking of Layers of Wood

The application video shows the palletizing of wood in a large sawmill and woodworking company. An industrial robot, equipped with the large-area vacuum gripping system FX from J. Schmalz GmbH, lifts complete layers of individual wooden boards from a conveyor belt and stacks them.

Large-area vacuum gripping system SBX

The ideal solution for difficult surfaces

The large-area vacuum-gripping system system SBX is intended primarily for the woodworking industry and is used to lift complete layers of planed beams.

Vacuum Crossbeam with FX 120/60

Fully Automated Loading of Stationary CNC Machine

This application example shows a solution for the fully automatic loading of a stationary CNC machine. The furniture parts, with varying dimensions, are lifted with only one vacuum crossbeam.



Further information:

Availability and price check
Vacuum components, clamping systems and workshop equipment


Direct order


Shopping cart

0Positions 0,00 €

Schmalz Media Center

Vacuum Tube Lifter JumboFlex

You can find application videos for various industries demonstrating our vacuum tube lifters and vacuum lifting devices in the Schmalz Media Center.

More...